2020-11-13 6:31 AM
Dear Sir,
Debug and driver folders are not created in code generation
Debug option is also not highlighted in menu button.
Below is the screenshot of that
please help.
2020-11-23 6:46 AM
2020-11-29 2:18 AM
Hi @Byede.1
If you are using Proxy, you should go to windows==> Preferences ==> Network Connections then you have to fill in HTTP and HTTPS (Host and port).
If you don't use a Proxy, with Direct and Native "Active Provider", you don't have to fill in the fields (you have to leave them all empty).
Best regards,
Nesrine