2023-09-13 03:07 AM
Dear Community,
When comparing STM32L5x2 line with STM32U5x9 line I had the surprise to read in product selector's view:
Supply Current Run Mode (per MHz) typical:
- For STM32L5x2: 96
- For STM32U5x9: 26
Are these numbers correct?
If yes, what can explain those differences (nearly 4x) between the two lines of MCUs?
Kind regards,
dom
Solved! Go to Solution.
2023-09-13 03:18 AM - edited 2023-09-13 03:28 AM
2023-09-13 03:18 AM - edited 2023-09-13 03:28 AM
2023-09-13 05:53 AM
2023-09-25 07:35 AM
Thanks @Sarra.S and @Issamos for your answers.
I think that what puzzled me if that they were both shown as ultra-low power microcontrollers, at various places. In the end, it was hard to catch the real differences between the two lines. It's now much more clear.
Again, thank you both for your support.
2024-09-05 02:50 PM
I find it interesting that the STM32U545 is listed as using more power in almost low-power modes also supported by the STM32L562, but the power per MHz is much, much lower. It seems that for battery powered applications where the CPU only wakes up for external events or timer expiration, the L5 may be better than the U5.