2023-09-13 03:07 AM
Dear Community,
When comparing STM32L5x2 line with STM32U5x9 line I had the surprise to read in product selector's view:
Supply Current Run Mode (per MHz) typical:
- For STM32L5x2: 96
- For STM32U5x9: 26
Are these numbers correct?
If yes, what can explain those differences (nearly 4x) between the two lines of MCUs?
Kind regards,
dom
Solved! Go to Solution.
2023-09-13 03:18 AM - edited 2023-09-13 03:28 AM
2023-09-13 03:18 AM - edited 2023-09-13 03:28 AM
2023-09-13 05:53 AM
2023-09-25 07:35 AM
Thanks @Sarra.S and @Issamos for your answers.
I think that what puzzled me if that they were both shown as ultra-low power microcontrollers, at various places. In the end, it was hard to catch the real differences between the two lines. It's now much more clear.
Again, thank you both for your support.