User Activity

When I'm building some of the demo projects, I often have this build error, which other developers have already reported in this community.And I followed the instructions on this link, and "patched" the msys-1.0.dll which is causing this crash at bui...
Hi,Under TouchGFX designer application there is an advertisement touting "STM32U599 fully supported" with an image of the kit with the rounded display. I got the kit from ST (STM32U5A9J-DK / DK32U5A9J$AT1) with the STM32U5A9, with the same round disp...
Hi,I'm running the latest release 6.9.2 of STM32CubeMx with admin rights. When I'm going into the install/remove packages and scroll down to the X-CUBE-TOUCHGFX package, the latest release 4.22.1 does not appear, even after a press on "Refresh" butto...
Dear Community,When comparing STM32L5x2 line with STM32U5x9 line I had the surprise to read in product selector's view:Supply Current Run Mode (per MHz) typical:- For STM32L5x2:    96- For STM32U5x9:   26Are these numbers correct?If yes, what can exp...
Kudos from
Kudos given to