2015-11-30 03:57 AM
CubeMx generates stm32f0xx_hal_adc_ex.h
In that file in the implementation of macro ADC_CHANNEL_INTERNAL_PATH the returned value is either ADC_CCR_TSEN or ADC_CHANNEL_VREFINT. The second is probably wrong and should be ADC_CCR_VREFEN. #bug #stm32f0 #adc-hal2015-11-30 04:45 AM
Hi ladyzhenskyy.yur.001,
Thanks for highlighting this issue. It is a known bug, but the fix has not yet been released on the web. It will be available in one of coming releases of the STM32cubeF0 package.Check this [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/STM32Cube_FW_F0_V1.3.0%20BUG%20reportfix&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21¤tviews=9]thread.-Syrine-