2020-02-25 01:11 AM
Hello I will use these crystals for STM32L4R9AII6
HSE Crystal 16MHz ±10ppm 8pF 60 Ohms (with external capacitors of 6pf (assuming stray capacitance of 5pf) and ext resistor of 1.6KOhm)
RTC CRYSTAL 32768Hz 9pF 20PPM (with external capacitors of 12pf)
https://www.digikey.com/product-detail/en/epson/FC-135-32.7680KA-AC/FC-13532.7680KA-AC-ND/1927426
Is these crystal suitable for this MCU and my values for the external capacitors and resistor correct?
Thanks in Advance!
2020-02-25 06:03 AM
Hello,
Both crystals are compatible with STM32L4R9. Also the chosen values of the external capacitors is good.
Please refer to AN2867 (Oscillator design guide for STM8AF/AL/S, STM32 MCUs and MPUs) for more details.
Best regards
Bouraoui