cancel
Showing results for 
Search instead for 
Did you mean: 

Could the STM32F103 or STM32F412 support 4GB eMMC nand flash?

HungKai.Chien
Associate II

Our project want to use the 4GB eMMC NAND Flash on STM32F103RC or STM32F412VE.

The eMMC architecture of NAND flash support revision , below. It just require to over the MMC standard 4.41 / 5.1.

Could the STM32F103RC or STM32F412VE support 4GB eMMC NAND flash?

2 REPLIES 2
TDK
Guru

Both of them have the hardware to support 4GB eMMC. The HAL support may not be complete. Last I checked the F4 only supported up to 2GB.

If you feel a post has answered your question, please click "Accept as Solution".

Yes, both F1 and F4 should be capable of accessing an eMMC device. You'll be responsible for implementing the driver.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..