2024-05-29 3:56 AM
Dear community,
I have faced with the problem in our developed boards with STM32F407 MCU. The firmware is based on FreeRTOS, vector table is located as usually in the beginning of 0x08000000 (see part of list file below).
Idx Name Size VMA LMA File off Algn
0 .isr_vector 00000188 08000000 08000000 00010000 2**0
CONTENTS, ALLOC, LOAD, READONLY, DATA
Boards with MCU are flashed with USB-UART adapter and STM32 Flash loader demonstrator https://www.st.com/en/development-tools/flasher-stm32.html
Boards have some parameters (configuration of sensors), stored in the Flash memory, so we used sector 7 for these data, and customer can update the information about these sensor parameters. Mainly boards works well, but some of them were returned from the customer as "works well, but now don't works at all". After reading the memory damp and comparison with reference board with the same firmware that works perfect, I have found that some memory area is corrupted, and it is only in vector table area - sector 0.
Some observations:
It seems to me, that it is not a problem with my software, but rather some problems with the microcontrollers. Have any faced with the same issue?
Solved! Go to Solution.
2024-06-09 3:15 AM
It looks like the source of the problem has been identified, and some solution was found. I have thoroughly investigated three boards with the issue of corrupted flash in sector 0. I have re-flashed them, firstly with the normal procedure that was used in the company ("STM32 Flash loader demonstrator" https://www.st.com/en/development-tools/flasher-stm32.html) with default parameters - no flash protection, BOR level not set (I assume, in this case it has level "off"). Then I have used STM32 CubeProgrammer software, and used the same parameters. You can find the results in the table below - they are marked as "attempt 2". As you can see, the boards were "broken" (corrupted sector 0 with set to "0" of some bits in the part of vector table). In the beginning, all three boards work, but then I have started to set the power on and off (I have used just rocker switch for power supply). The number of power on-off cycles, which board works was different - from 10 to 58. In the end, all three boards were with corrupted flash in sector 0. I have played with the software (I have used CubeProg as well as Demonstartor), and with option bits (the write protection of sectors, as well as brownout reset BOR level). It become clear, that solution proposed here https://community.st.com/t5/stm32-mcus-products/powering-cycling-stm32f4-board-corrupts-flash-programming/m-p/552257/highlight/true#M208631 (set BOR level to 3 and protect it from writing Flash sectors) is only partially correct. In fact, writing protection doesn't help at all - with BOR level OFF the boards were broken even with protected sectors. The only solution is to set BOR level to 3 - in this case all three boards survived 200 cycles of power on-off and then I have not continued testing to not waste a time.
So, it means that STM has some issue with at least STM32F407 MCU (in my case as well as in the case described by the link above the MCU was the same - STM3F407). The Flash memory can be corrupted in Sector 0 (default vector table) when the BOR level is off, and reset of MCU become at low voltage. To solve the issue, BOR level should set at level 3, with minimum threshold voltage 2.75...2.85 V. Maybe it will also work to set lover level (1 or 2), but I have decided that in my case it works and have not analyzed it further.
Brd. | Attempt | Software | BOR value (level) | WP Sectors 0…6, 8…11 | On-off # | Result |
1 | 2 | CubeProg. | 3 (OFF) | Not active | 58 | Corrupted sector 0 |
1 | 3 | Demonstrator | 3 (OFF) | Not active | 78 | Corrupted sector 0 |
1 | 4 | Demonstrator | 3 (OFF) | Active | 11 | Corrupted sector 0 |
1 | 5 | CubeProg. | 0 (3) | Active | 200 | Ok |
2 | 2 | CubeProg. | 3 (OFF) | Not active | 10 | Corrupted sector 0 |
2 | 3 | CubeProg. | 3 (OFF) | Not active | 40 | Corrupted sector 0 |
2 | 4 | CubeProg. | 0 (3) | Active | 200 | Ok |
3 | 2 | CubeProg. | 3 (OFF) | Active | 48 | Corrupted sector 0 |
3 | 3 | CubeProg. | 0 (3) | Not active | 200 | Ok |
2024-05-29 4:09 AM
Writing blocks of zeros, whilst leaving original content elsewhere is very odd.
The write functions as a write-once, so unlike more classic FLASH chips you can't keep knocking down ONE bits.
Double check your VCAP capacitors.
Remove your flashing code and see if you can replicate.
2024-05-30 4:58 AM
We also experenced exactly the same issue. The starting part of the flash is set to be all 0, as shown below,
as the vector table is filled with 0, the mcu cannot be booted now.
2024-06-03 1:53 AM
Hi all,
I will try to use the solution proposed here https://community.st.com/t5/stm32-mcus-products/powering-cycling-stm32f4-board-corrupts-flash-programming/m-p/552257/highlight/true#M208631, it looks like the issue is not new, but it is strange that ST has not paid attention to it. Anyway, it is not so easy to represent this issue with corrupted flash in a lab, because not all boards from customers returned with it, many work well during a long time...
2024-06-09 3:15 AM
It looks like the source of the problem has been identified, and some solution was found. I have thoroughly investigated three boards with the issue of corrupted flash in sector 0. I have re-flashed them, firstly with the normal procedure that was used in the company ("STM32 Flash loader demonstrator" https://www.st.com/en/development-tools/flasher-stm32.html) with default parameters - no flash protection, BOR level not set (I assume, in this case it has level "off"). Then I have used STM32 CubeProgrammer software, and used the same parameters. You can find the results in the table below - they are marked as "attempt 2". As you can see, the boards were "broken" (corrupted sector 0 with set to "0" of some bits in the part of vector table). In the beginning, all three boards work, but then I have started to set the power on and off (I have used just rocker switch for power supply). The number of power on-off cycles, which board works was different - from 10 to 58. In the end, all three boards were with corrupted flash in sector 0. I have played with the software (I have used CubeProg as well as Demonstartor), and with option bits (the write protection of sectors, as well as brownout reset BOR level). It become clear, that solution proposed here https://community.st.com/t5/stm32-mcus-products/powering-cycling-stm32f4-board-corrupts-flash-programming/m-p/552257/highlight/true#M208631 (set BOR level to 3 and protect it from writing Flash sectors) is only partially correct. In fact, writing protection doesn't help at all - with BOR level OFF the boards were broken even with protected sectors. The only solution is to set BOR level to 3 - in this case all three boards survived 200 cycles of power on-off and then I have not continued testing to not waste a time.
So, it means that STM has some issue with at least STM32F407 MCU (in my case as well as in the case described by the link above the MCU was the same - STM3F407). The Flash memory can be corrupted in Sector 0 (default vector table) when the BOR level is off, and reset of MCU become at low voltage. To solve the issue, BOR level should set at level 3, with minimum threshold voltage 2.75...2.85 V. Maybe it will also work to set lover level (1 or 2), but I have decided that in my case it works and have not analyzed it further.
Brd. | Attempt | Software | BOR value (level) | WP Sectors 0…6, 8…11 | On-off # | Result |
1 | 2 | CubeProg. | 3 (OFF) | Not active | 58 | Corrupted sector 0 |
1 | 3 | Demonstrator | 3 (OFF) | Not active | 78 | Corrupted sector 0 |
1 | 4 | Demonstrator | 3 (OFF) | Active | 11 | Corrupted sector 0 |
1 | 5 | CubeProg. | 0 (3) | Active | 200 | Ok |
2 | 2 | CubeProg. | 3 (OFF) | Not active | 10 | Corrupted sector 0 |
2 | 3 | CubeProg. | 3 (OFF) | Not active | 40 | Corrupted sector 0 |
2 | 4 | CubeProg. | 0 (3) | Active | 200 | Ok |
3 | 2 | CubeProg. | 3 (OFF) | Active | 48 | Corrupted sector 0 |
3 | 3 | CubeProg. | 0 (3) | Not active | 200 | Ok |