SPI slave issue
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-08 11:33 PM
Hello
I am using 2 boards with SPI communication between them: STM32F412G-DISCO as the master, NUCLEO-G071RB as the slave. The MOSI direction works well, but the MISO direction doesn't works. Monitoring the MISO line via. oscilloscope shows that there is no communication in this line, also it is expected to be.
The boards configuration:
The master code:
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_2, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi1, (uint8_t *)&spi_tx, 2,100);
HAL_SPI_Receive(&hspi1, (uint8_t *)&spi_rx, 2,100);
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_2, GPIO_PIN_SET);
The slave code:
HAL_SPI_Receive_IT(&hspi1,(uint8_t *)&spi_rx,2);
HAL_SPI_Transmit_IT(&hspi1, (uint8_t *)&spi_tx,2);
void HAL_SPI_RxCpltCallback (SPI_HandleTypeDef * hspi) {
counter++;
if (counter==10) {
counter=0;
}
sprintf(spi_tx,"c%d",counter);
for(int i=0;i<4;i++) {
spi_buf[counter*2+i]=spi_rx[i];
}
HAL_SPI_Receive_IT(&hspi1,(uint8_t *)&spi_rx,2);
}
void HAL_SPI_TxCpltCallback (SPI_HandleTypeDef * hspi) {
HAL_SPI_Transmit_IT(&hspi1, (uint8_t *)&spi_tx,2);
}
Does anyone have a suggestion what is the problem?
- Labels:
-
STM32F4 Series
-
STM32G0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-09 12:17 AM
Hi,
1. for transmit + receive (at same time) use : HAL_SPI_TransmitReceive_IT(..);
2. just for transmitting 2 bytes : why not set the spi to 16bit and do it in one spi transfer?
3. using NSS hardware on receiver, but nss-software on transmitter...might create problem, if you dont do in software, what other chip spi-hardware expects. Try setting both to hardware nss. And use TransmitReceive on both sides.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-09 12:36 AM
Hi,
I tried your suggestion, now the slave indicates that the Busy flag is set, and the HAL_SPI_TxRxCpltCallback doesn't called back.
general question: is the HAL_SPI_TransmitReceive_IT(..) works also when the number of bytes differ for the transmit and receive directions?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-09 1:25 AM - edited ‎2024-06-09 1:33 AM
No. SPI is more or less just a serial shift register, so what you shift IN (bits number), will come out.
So one master-slave TransmitReceive is like : exchanging the spi values master <--> slave.
Number of bytes always same for the transmit and receive directions.
If you want receive 3 bytes, but have only 1 (command or..) to send, you have to send 3 , even 2 are 00 or whatever.
Because you want 3x spi transfer action.
And think about timing : when master shifts spi, slave has to shift out data, without any delay - if "you" (=slave) is ready - or not.
So slave needs to be "faster" than master, always having the needed data ready for transfer, if a transfer "might" come.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-09 1:33 AM
I understand what you are saying for the general question. So if I want to transfer different number of bytes, I should use HAL_SPI_Transmit (); HAL_SPI_Receive (); in the master, and 2 interrupts in the slave.
Again, my problem is that the MISO transmit doesn't works, and when I am trying to force it (manually or using the HAL_SPI_TransmitReceive_IT (); function) the bus stays busy (Busy flag kept set).