cancel
Showing results for 
Search instead for 
Did you mean: 

Confirmation on EXTI limitiation

sarun
Associate III

I want to confirm the limitations of GPIO interrupts on STM32 devices.

I am using an STM32H7 device, and observed that interrupts cannot be configured for PA0 and PB0 at the same time.  I could not find any confirmation regarding this in the device datasheet,can anyone give me the confirmation on this.

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @sarun ,

If you refer to the reference manual / SYSCFG_EXTICR[n] register, you find that only one IO on x position could be configured as EXTI input at a time:

SofLit_0-1732872386323.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

3 REPLIES 3
STTwo-32
ST Employee

Hello @sarun 

PA0 and PB0 and so on, are connected to Line0, so you can use only one pin at one time to handle interrupt from there.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

SofLit
ST Employee

Hello @sarun ,

If you refer to the reference manual / SYSCFG_EXTICR[n] register, you find that only one IO on x position could be configured as EXTI input at a time:

SofLit_0-1732872386323.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
sarun
Associate III

Thank you for the support  @SofLit  @STTwo-32