cancel
Showing results for 
Search instead for 
Did you mean: 

Composite USB with CDC and HID

180794
Associate
Posted on July 14, 2014 at 14:21

Hi,

I would like to create device with CDC (Virtual COM) and HID classes. I am inspired by mass memory and hid composite example.For creating composite devices is two ways:

1. Use IAD class, but it is not supported in Windows 8: msdn.microsoft.com/en-us/library/windows/hardware/ff540054(v=vs.85).aspx

2. Write descriptors with two independent interfaces.

I chose second way. HID device is detected  well, but Virtual COM is not working, even I try install driver (the same as ST provides for Virtual COM example - obviously VID and PID was changed properly).

I attached desciptor from USBlyzer and screenshot of device manager.

Some ideas?
0 REPLIES 0