cancel
Showing results for 
Search instead for 
Did you mean: 

Compilation error : internal segmentation fault with GNU Toolchain 11.3.Rel1 for STM32U5

SauravShandilya
Associate

Hello Community,

 

I am getting internal compiler error: Segmentation fault when optimization is set to O2 or O3. I am using GNU C17 (Arm GNU Toolchain 11.3.Rel1) version 11.3.1 20220712 toolchain. 

I am compiling code for STM32U575ZI MCU. Compilation goes through without error when optimization is set to O0 or O1. As soon as Optimization is set to O2 and above, I see the compiler error: internal segmentation fault. Below is screenshot of error. Also attached is compilation log.

InternalSegmentationFault_O2.jpg

 

Can someone tell the reason for internal Segmentation fault and help to fix it?

 

Best Regards

Saurav

3 REPLIES 3
CMYL
ST Employee

Hello @SauravShandilya 

To reproduce the issue, I used the DMA_LinkedList example of the STM32U5CubeFW:

(~\STM32Cube_FW_U5_V1.4.0\Projects\NUCLEO-U575ZI-Q\Examples\DMA\DMA_LinkedList)

I'm using  C/C++ ARM GNU Toolchain version 11.3.0.202307110141, I tried all the optimization options and it is working on my side. By comparing the compilation flags versus the one you shared shared, I see that you enabled both '-D' 'USE_FULL_LL_DRIVER' '-D' 'USE_HAL_DRIVER'

  • Can you check with only keeping '-D' 'USE_FULL_LL_DRIVER'
  • Can you also add the following option to compilation:   -std=gnu11

 

Best Regards,

Younes

Hi @CMYL ,

 

Thank you for sharing a response. 

 

I removed -DUSE_HAL_DRIVER and added -std=gnu11 in compilation flag. However, that did not resolve the issue on my side.

 

I can notice the difference in Toolchain version. You are using 11.3.0 whereas I am using 11.3.Rel1. As per Arm GNU Toolchain Downloads – Arm Developer 11.3.0 can not be download and I am using 11.3.Rel1 in production code which is difficult to change.

Can you check with same Toolchain which I am using, which is 11.3.Rel1. Below is link of toolchain: 

https://developer.arm.com/-/media/Files/downloads/gnu/11.3.rel1/binrel/arm-gnu-toolchain-11.3.rel1-mingw-w64-i686-arm-none-eabi.zip?rev=82f0e95b5a7740d9899e6ce375df8106&hash=279E24D725F493C4E3B90C8B2A159813A91CD29C

 

Best Regards

Saurav

 

jcjunker
Associate II

@SauravShandilya @CMYL Was there any resolution to this issue? I am having the same problem occur when using STM32CubeCLT 1.15.1 when building in Release. I see that my compiler version is also 11.3.1.Rel1. I'd like to get this resolved so that I can continue using STM32CubeCLT with the VS Code extension, and not have to move to an externally managed compiler version.

 

- Jacob