User Activity

I am trying to enter USART1 bootloader (Pin PC4 and PC5) for STM32G474RCT6 MCUWe are following AN2606 and tried to keep the option bit configurations as per the highlighted row under pattern 14Bit status:The Boot0 pin (PB8) is NOT  pulled down with r...
Hello, I am trying to flash the MCU with USART bootloaderI am using the command codes from below link, but are not working for meCan someone help me validate of the command codes are correct for STM32G4https://www.st.com/resource/en/application_note/...
Hi,Is there a sample code to control the STM32 motor board with UART from a host PCI'm mostly looking for setting and getting the encoder angles and speed control with the UART 
Hello,I am trying to use the MC SDK v6.2.0 for controlling a PMSM and I wish to control the motor through my host PC with uart protocolI have got below document which is for SDK v4.3.Can you please share similar user manual for SDK v6.2.0Can you also...