Command sequence for USART bootloader on stm32G4 MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-13 6:54 AM
Hello,
I am trying to flash the MCU with USART bootloader
I am using the command codes from below link, but are not working for me
Can someone help me validate of the command codes are correct for STM32G4
Current setup:
I have connected the STM32 USART4 to my R PI device. It gets enumerated as /dev/ttyUSB0
Below is the serial code using python
TIA
Solved! Go to Solution.
- Labels:
-
STM32G4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-13 9:30 AM - edited ‎2024-05-13 9:31 AM
Nice catch @Tesla
Even you didn't mention the exact G4 part number but UART4 is not used for G4 bootloader.
You can refer to the AN2606 tables Table 99 / Table 101 / Table 103: Only USART1, 2 and 3 are used for bootloader.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-13 7:56 AM
Going to be as described in AN2606 for the pins and AN3155 for the UART
Pretty sure UART4 has NO involvement, read and understand expectation from AN2606..
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
‎2024-05-13 9:30 AM - edited ‎2024-05-13 9:31 AM
Nice catch @Tesla
Even you didn't mention the exact G4 part number but UART4 is not used for G4 bootloader.
You can refer to the AN2606 tables Table 99 / Table 101 / Table 103: Only USART1, 2 and 3 are used for bootloader.