cancel
Showing results for 
Search instead for 
Did you mean: 

CMSIS STM32 detailed description.

lipin
Associate II
Posted on July 12, 2010 at 19:01

CMSIS STM32 detailed description.

1 REPLY 1
swhite2
Associate III
Posted on May 17, 2011 at 13:58

Firstly a terminology quibble. CMSIS (Cortex Microcontroller Software Interface Standard ) refers to the ARM part of the library. The peripheral stuff is unique to ST.

The Standard Peripheral library Documentation leaves a lot to be desired and probably everyone here agrees with that.However it is what it is so you still have to read the

http://www.st.com/mcu/files/mcu/1221142709.pdf

to understand the peripherals and how they work.

Personally I prefer to use the library most of the time but I don't need to toggle port pins at 20MHz etc so it works fine for me. However your mileage may vary.