2010-07-12 10:01 AM
CMSIS STM32 detailed description.
2011-05-17 4:58 AM
Firstly a terminology quibble. CMSIS (Cortex Microcontroller Software Interface Standard ) refers to the ARM part of the library. The peripheral stuff is unique to ST.
The Standard Peripheral library Documentation leaves a lot to be desired and probably everyone here agrees with that.However it is what it is so you still have to read the to understand the peripherals and how they work. Personally I prefer to use the library most of the time but I don't need to toggle port pins at 20MHz etc so it works fine for me. However your mileage may vary.