Character match on STM32F303K8
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-11 9:34 AM
Hello,
I'm trying to set up the character match interrupt to detect the character '\n' (which indicates the end of a packet) and I don't manage to get the interruption.
The procedure I'm using is:
- initialize the uart, its gpios, and the dma.
- enable the uart as well as dma interrupt in NVIC
- disable uart
- write \n into CR2_ADD
- write to 1 CR1_CMIE
- enable uart
- HAL_UART_Receive_DMA
- in the USARTx_IRQHandler I check the ISR_CMF flag, and if it is not zero I call my routines to handle the input-
By doing this on UART1 I don't get any UART interrupt. I just see the dma TC interrupt when the buffer is full.
I also tried with HAL_UART_Receive_IT (i.e. without the DMA) with similar results.
Now I'm considering that I might misunderstood the specifications and maybe the stm32f303k8 doesn't support character match, or maybe some limitation applies to it. Is this the case?
The datasheet clearly states that Modbus communication is supported only on UART1 (which is the one I'm using), and the manual states that Modbus support includes timeout and CR/LF character recognition, therefore everything looks correct but I get no interruption with '\n'.
Any suggestion?
Thank you,
Davide.
Solved! Go to Solution.
- Labels:
-
STM32F3 Series
-
UART-USART
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-13 2:23 AM
OMG, I feel so stupid.
I just checked, and the terminal send the \r (and not \n)!! Now I changed the character to \r and the interruption works!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-12 2:14 AM
Are you sure the mcu is receiving the character want to use as trigger? Can you confirm this by a polled receiver with the same settings?
Also read back check the content of USART registers.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-12 2:22 AM
So, before trying with the CM interrupt I used to manually check char-by-char on RXNE interrupt in order to detect the \n, it worked perfectly when I manually enter the data in a serial terminal (then the \n is there in the uart stream).
Now I need to use the CM interrupt because the data is transmitted in automatic fashion using a python script, therefore bytes are transmitted much faster (same baudrate but shorter inter character interval) and the mcu somehow miss the \n. I suppose it is because of overrun problem.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-12 3:58 AM
As I've said, read out and check/post the USART registers' content.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-12 4:39 AM
Oh yes, these are the values just before HAL_UART_Receive_DMA, CM interrupt should be enabled
USART1->CR1 = 0x0000400d
USART1->CR2 = 0x0a000000
USART1->CR3 = 0x00000000
USART1->BRR = 0x00000045
USART1->GTPR = 0x00000000
USART1->RTOR = 0x00000000
USART1->RQR = 0x00000000
USART1->ISR = 0x006000d0
USART1->ICR = 0x00000000
USART1->RDR = 0x00000000
USART1->TDR = 0x0000000a
After HAL_UART_Receive_DMA (when the interrupt is supposed to be fired) they are:
USART1->CR1 = 0x0000410d
USART1->CR2 = 0x0a000000
USART1->CR3 = 0x00000041
USART1->BRR = 0x00000045
USART1->GTPR = 0x00000000
USART1->RTOR = 0x00000000
USART1->RQR = 0x00000000
USART1->ISR = 0x006000d0
USART1->ICR = 0x00000000
USART1->RDR = 0x00000000
USART1->TDR = 0x0000000a
I hope the format is understandable, otherwise let me know if there is a better way to export it (I'm using arm gdb for debug).
Thank you,
Davide.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-13 2:23 AM
OMG, I feel so stupid.
I just checked, and the terminal send the \r (and not \n)!! Now I changed the character to \r and the interruption works!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-13 4:16 AM
Thanks for coming back with the solution. Please select your post as "Best" so that the thread is marked as solved.
JW
PS. I personally confuse \r <CR> \n<LF> all the time too...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-24 5:53 AM
Hello, one question to this regarding the commands:
- disable uart
- write \n into CR2_ADD
- write to 1 CR1_CMIE
- enable uart
Are there some HAL functions to control the registers. It is of course possible to set the register directly, but in terms of HW abstraction this is not the best solution. Or do I just overlook something?