cancel
Showing results for 
Search instead for 
Did you mean: 

Changing sample rate on streaming with H753 board

skson
Associate II

Hello, 
I am implementing audio streaming with H753 board.

My goal is like below.

skson_0-1745198527483.png

 

 


1. Input : USB connected PC,

which can be selected one of 48kHz and 44.1kHz sample rate on connecting state.

Others are fixed as 16 bit / 2 slot ( stereo )   

2. Output : 32 bit Stereo SAI(I2S). Sample rate is same to input.

 

3. What I have succeed :

Default streaming : Good Sound : [48kHz/16bit/Stereo USB]  to [48 kHz/32bit/Stereo SAI].

SAI output frequency of FS / SCK : Both 44.1kHz and 48kHz case.

 

4. Problems: 

The testing sound is always low tone after changed sample rate.

both [48k->44.1k, Test] and [44.1k->48k, Test] are same.   

skson_1-1745199713895.png

Could I get some help?

 

Thank you.

From Skson.

1 REPLY 1
FBL
ST Employee

Hi @skson 

Do you reproduce using a reference board? Can you configure your system to perform a loopback test where the audio data received via USB is sent back to the host PC without processing through the SAI to narrow down the issue?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL