cancel
Showing results for 
Search instead for 
Did you mean: 

Change Period/Pulse of HRTIM based SimplePWM

C-Coder
Associate II

Custom board, STM32H747 device, Simple PWM

 

Using the code generated by MX, and adding a call to HAL_HRTIM_SimplePWMStart, I can generate a nice simple PWM output signal. If I change the initial values for period/pulse, rebuild, and program to the device, I can see the changed output signal. Now I want to change the period and/or the pulse after it has started. I've tried this a few ways. one is:

 

    	// Update the period/pulse stored in the structs above...

    	__HAL_HRTIM_SETPERIOD(&hhrtim, HRTIM_TIMERINDEX_TIMER_A, g_TimeBaseCfg.Period);
    	__HAL_HRTIM_SETCOMPARE(&hhrtim, HRTIM_TIMERINDEX_TIMER_A, HRTIM_COMPAREUNIT_1, g_SimplePWMChannelCfg.Pulse);
    	HAL_HRTIM_SoftwareUpdate(&hhrtim, HRTIM_TIMERINDEX_TIMER_A);

 

I've also tried doing:

    	// Update the period/pulse stored in the structs above...

    	if (HAL_HRTIM_SimplePWMStop(&hhrtim, HRTIM_TIMERINDEX_TIMER_A, HRTIM_OUTPUT_TA1) != HAL_OK)
    	{
    		Error_Handler();
    	}

    	if (HAL_HRTIM_TimeBaseConfig(&hhrtim, HRTIM_TIMERINDEX_TIMER_A, &g_TimeBaseCfg) != HAL_OK)
    	{
    	  Error_Handler();
    	}
    	if (HAL_HRTIM_SimplePWMChannelConfig(&hhrtim, HRTIM_TIMERINDEX_TIMER_A, HRTIM_OUTPUT_TA1, &g_SimplePWMChannelCfg) != HAL_OK)
    	{
    	  Error_Handler();
    	}
    	if (HAL_HRTIM_SimplePWMStart(&hhrtim, HRTIM_TIMERINDEX_TIMER_A, HRTIM_OUTPUT_TA1) != HAL_OK)
    	{
    		Error_Handler();
    	}

 

Regardless of which method I try, the resulting output signal is still using the same period and pulse. Can any one name the one or hundred simple things I'm missing?

 

Thank you,

C-Coder

0 REPLIES 0