2025-03-17 2:41 PM
I'm having the same problem on 2 different boards. I gen'd up a simple program using CubeMX and I'm only sending some data to both ports at the same time:
void StartTask02(void const * argument)
{
/* USER CODE BEGIN StartTask02 */
/* Infinite loop */
int i;
for(i = 0;i < DATA_SIZE;i++)
data[i] = i;
vTaskDelay(1000);
for(;;)
{
vTaskDelay(2);
HAL_UART_Transmit(&huart1, &data[0], DATA_SIZE/5, 100);
HAL_UART_Transmit(&huart2, &data[0], DATA_SIZE/5, 100);
}
/* USER CODE END StartTask02 */
}
I thought maybe one was a 'knock-off' because the LED's aren't colored while the other is.
Solved! Go to Solution.
2025-03-17 3:05 PM - edited 2025-03-17 5:21 PM
See the document for your board, page 22. https://www.st.com/resource/en/user_manual/dm00039084-discovery-kit-with-stm32f407vg-mcu-stmicroelectronics.pdf
Pins PA9, PA10 are not free to use. They are connected to the green LED and USB.
Before assigning pins, check that these pins are free to use - even if they are routed to connector.
Try USART3 on TX PD8, RX PD9
2025-03-17 2:58 PM
Show circuit, what you connect to the boards, so its not only guessing...
+
On your scope pic : 50v/div + 5V/div -> about 30Vss + 15Vss signals , where you measure this ??
2025-03-17 3:05 PM - edited 2025-03-17 5:21 PM
See the document for your board, page 22. https://www.st.com/resource/en/user_manual/dm00039084-discovery-kit-with-stm32f407vg-mcu-stmicroelectronics.pdf
Pins PA9, PA10 are not free to use. They are connected to the green LED and USB.
Before assigning pins, check that these pins are free to use - even if they are routed to connector.
Try USART3 on TX PD8, RX PD9
2025-03-18 5:01 AM
I think you may be right. In the manual, I found this:
USB LD7: green LED indicates when VBUS is present on CN5 and is connected to PA9
of the STM32F407VGT6dm00039084-discovery-kit-with-stm32f407vg-mcu-stmicroelectronics.pdf on page 18/32
2025-03-18 5:02 AM
I just had the scope probes hooked up to TX of UART1 & 2. I didn't bother to set the voltages.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.