‎2022-10-31 11:14 PM
Hello
I use the embedded Op Amp in STM32U585VIT3Q to charge a 47uF capacitor.
The input of the Op Amp is connected to the output of DAC. The voltage level is 3V.
So you can see when the Op Amp begin to charge the cap, the peak current is quite large.
I would like to know whether the Op Amp or the Micro could withstand this pulse current
Thanks in advance!
Solved! Go to Solution.
‎2022-11-02 5:55 PM
Hello Peter
Thanks. I was not aware of the problem of using email to reply. It is OK for you to remove the info.
:grinning_face: :grinning_face: