2024-06-03 3:02 PM
I seem to remember a way to make a reset event set a timer’s value to a non-zero value. However, I didn’t see anything in the docs for the part I’m using so I’m not sure if this is a feature in STM32 parts. Is it?
An alternative is a DMA trigger on the reset that loads the CNT value. Is there a better way?
I have an in input capture value that represents a signed value. If a 16 bit timer resets to a value above 65535/2, input capture values within a known range can be sent away via DMA to the FMAC without processing steps to sort out the sign.
Solved! Go to Solution.
2024-06-21 12:43 PM
I don't think that accomplishes what I need. I'd need an auto-reload value and then a value other than zero to specify as the value to be reloaded. Looks like DMA is the only way.
2024-06-06 2:30 AM
Check "Downcounting mode" :
In downcounting mode, the counter counts from the auto-reload value (content of the
TIMx_ARR register) down to 0, then restarts from the auto-reload value and generates a
counter underflow event.
2024-06-21 12:43 PM
I don't think that accomplishes what I need. I'd need an auto-reload value and then a value other than zero to specify as the value to be reloaded. Looks like DMA is the only way.