Skip to main content
RShan
Associate
June 27, 2023
Question

CAN RX interrupt invokes LTDC error upon exit

  • June 27, 2023
  • 1 reply
  • 656 views

This is a weird one :) I'm using the STM32F769 device, and I have the LTDC peripheral running at low speed (8MHz PCLK). When I send a CAN message to the unit, the CAN RX interrupt is invoked, and only when the ISR exits,  an LTDC error interrupt is raised, which indicates FIFO underrun. Here is a code snippet below:

void conv_u32_to_buf(uint32_t num, uint8_t buf[])
{
   memcpy(buf, (void*)&num, 4);
}

void CAN1_RX0_IRQHandler(void)
{
   CAN_TypeDef* can = CAN1;

   // If CAN message available in the FIFO
   if ((can->RF0R & CAN_RF0R_FMP0) != 0U)
   {
      uint8_t data[8];

      // Get pointer to mailbox
      CAN_FIFOMailBox_TypeDef* mailbox = &can->sFIFOMailBox[CAN_FILTER_FIFO0];
  
      // This does not work
      uint32_t tmp = mailbox->RDLR;
      conv_u32_to_buf(tmp, &data[0]);
      tmp = mailbox->RDHR;
      conv_u32_to_buf(tmp, &data[4]);

      // This works
      //tmp = mailbox->RDLR;
      //memcpy(&data[0], &tmp, sizeof(uint32_t));
      //tmp = mailbox->RDHR;
      //memcpy(&data[4], &tmp, sizeof(uint32_t));
  
      // Dequeue the message from the peripheral, as we have wha
      can->RF0R |= CAN_RF0R_RFOM0;
  }

}

Interesting Note #1: If I do the memcpy directly in the ISR, there is no issue, but if I call conv_u32_to_buf, passing in num by value, it invokes the error

Interesting note #2: If I change conv_u32_to_buf so that pointer to num is passed if, there is no error.

Interesting note #3: the NVIC priorities for LTDC are 0-0 (preemptive, sub-priority), and CAN RX are 0-1

CAN is on a lower sub-priority, and the LTDC does not interrupt it

Interesting note #4: The same code on the STM32F469 does not raise an LTDC error. The M4 platform has worked well for us for 5 years.

So any ideas as to why this is failing on the M7 device? Silicone bug, or perhaps something I'm missing, o are not aware of?

Rob

This topic has been closed for replies.

1 reply

mƎALLEm
ST Technical Moderator
September 22, 2026

Hello,

It’s a bad idea to start with baremetal coding. 

Start with HAL, validate your application then optimize it with baremetal coding. 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.