This is a weird one I'm using the STM32F769 device, and I have the LTDC peripheral running at low speed (8MHz PCLK). When I send a CAN message to the unit, the CAN RX interrupt is invoked, and only when the ISR exits, an LTDC error interrupt is ra...