cancel
Showing results for 
Search instead for 
Did you mean: 

Can I use VOS0 for low clock speeds?

tjdyhdsfeadgstdj
Associate III

I'm working on an application that requires a very fast UART speed. The STM32H7 allows a UART speed of 17 Mbps, which is just barely enough, but should work. However, other than the fast UART speed, I don't need to do a lot of processing. I would have much preferred to use an ultra-low-power device instead.

Because of this I want to run the MCU clock speed as low as possible. However, using CubeMX and the clock configuration tool, I'm running into issues where when I drop the CPU clock, the maximum speed of the UART peripheral clock drops too low for my needs. I've traced this down to what I believe is a voltage scaling "VOS" issue. Each VOS voltage scaling value places a limit on the maximum UART speed (see General operating conditions table, fpclk value).

So my question is basically, Could I run the CPU at 140 MHz (which seems to recommend VOS3) but set VOS to VOS0, which would allow the 17 Mbps UART speed? Or do I need to us VOS3 with that low of a CPU clock? Are there any issues I should be aware of with doing this?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Super User

afaik you can use any vos , to get it switch faster. no need, to use the highest possible core speed.

+

where you see this 17Mb limit ?

in H743 ds is:  12,5 Mb

AScha3_0-1696099995910.png

for your need, the new H503 seem better (cheaper + faster):

AScha3_1-1696100080072.png

+ available...

https://www.mouser.de/ProductDetail/STMicroelectronics/STM32H503CBT6?qs=amGC7iS6iy99sz%2FXgeIPHg%3D%3D

 

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
AScha.3
Super User

afaik you can use any vos , to get it switch faster. no need, to use the highest possible core speed.

+

where you see this 17Mb limit ?

in H743 ds is:  12,5 Mb

AScha3_0-1696099995910.png

for your need, the new H503 seem better (cheaper + faster):

AScha3_1-1696100080072.png

+ available...

https://www.mouser.de/ProductDetail/STMicroelectronics/STM32H503CBT6?qs=amGC7iS6iy99sz%2FXgeIPHg%3D%3D

 

 

If you feel a post has answered your question, please click "Accept as Solution".

Thank you! I will also look at the new part.

An example of the 17 Mbps is the STM32H725. In the datasheet Electrical characteristics > operating conditions > communication interfaces, USART characteristics, fck USART clock frequency is listed as 17 MHz in Master mode.