cancel
Showing results for 
Search instead for 
Did you mean: 

Steval-Proteus 1 Data Logging Projects from Git Hub Do Not Work

Garnett.Robert
Senior III

Hi

I used Git Hub to download:

https://github.com/stm32-hotspot/stm32ai-nanoedge-datalogger

1. I then built all projects error free with STM32CubeIDE. 

2. I then used my STlink MINIE to program my Steval Proteus1 with STEVAL-PROTEUS1_ISM330DHCX

3. I started Terra Terminal and connected to the USB-Serial CH340 (COM9) set to 115200 8, none, 1

4. I didn't get any response.

5. I entered the debugger and found that the project was stalling on line 581 main.c: HAL_Delay(10);

 

 

 

 

static void ism330dhcx_initialize_basics()
{
  /* Check device ID */
  whoamI = 0;

  do {
    /* Wait sensor boot time */
    HAL_Delay(10);  /* Stalled here - no systick interrupts?? */
    ism330dhcx_device_id_get(&dev_ctx, &whoamI);
  } while (whoamI != ISM330DHCX_ID);

  /* Restore default configuration */
  ism330dhcx_reset_set(&dev_ctx, PROPERTY_ENABLE);

  do {
    ism330dhcx_reset_get(&dev_ctx, &rst);
  } while (rst);

  /* Start device configuration. */
  ism330dhcx_device_conf_set(&dev_ctx, PROPERTY_ENABLE);
}

 

 

 

6. I then tried the other Proteus project: STEVAL-PROTEUS1_IIS3DWB

Similar problems.

 

I got rid of HAL_Delay with time delay loops, but it never got past: if (drdy) {

 

 

  while (1)
  {
    uint8_t wtm_flag = 0, status2 = 0;
    uint16_t num = 0;
    if (drdy) {
      /* Reset data ready contition */
      drdy = 0;
      ism330dhcx_read_reg(&dev_ctx, ISM330DHCX_FIFO_STATUS2, &status2, 1);
      wtm_flag = status2 >> 7;
      if (wtm_flag) {

 

 

Can anyone help here?

Best regards

Rob

 

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0