cancel
Showing results for 
Search instead for 
Did you mean: 

Bug Repport: CubeMX 4.16.0 DMA ''Use FIFO'' Checkbox stuck

ayarema
Associate II
Posted on August 10, 2016 at 23:11

Using CubeMX version 4.16.0 with DMA it does not let you turn off FIFO mode. The check mark does not deselect. 

0690X00000604vAQAQ.png

The generated source code needs to be manually modified to turn off FIFO. After the following change the DMA works properly.

0690X00000604v6QAA.png

#!stm32-!cubemx-!bug-!dma
3 REPLIES 3
Nesrine M_O
Lead II
Posted on August 11, 2016 at 11:07

Hi yarema.andriy ,

Could you please precise which STM32 product are using? So that it will be easier to verify the issue?

-Syrine-

ayarema
Associate II
Posted on August 11, 2016 at 19:06

The CubeMX is used to generate code for the STM32F767 Nucleo Board. Same issue was seen when it was used for STM32F746 Nucleo Board.

Nesrine M_O
Lead II
Posted on August 12, 2016 at 11:06

Hi  yarema.andriy,

I'll report this issue to our MX team for checking. Sorry for the inconvenience it may bring.

-Syrine-