2014-10-02 4:12 PM
Hello! I`m
use
STM32_USB-Host-Device_Lib_V2.1.0
and
try to run the
USB
audio device
on
STM32F407VE + USB3300,
the device
is properly detected
and
any
audio player
starts
playing
, but the data
did not
come
as soon as
passed
initialization
EP1 (OUT)
are beginning to
be called
one after another
interrupt
Incomplete isochronous
OUT data transfers interrupt (IISOOXFRM in OTG_HS_GINTSTS),
data on the
EP1
as a consequence
do not come.
Tried
a lot of things
to do
but nothing helps
:(
may
have any
or
especially when working
with
isochronouspoints
in
HS mode with external PHY?
Hardware problems
virtually
rule
,since
successfully
launched
VCP
inHS mode,
the data is transmitted
normally
, the example
works fine.
I would be very
grateful for any
hint
, thanks in advance!2014-10-04 9:38 PM
2016-08-11 7:39 PM