Bootloader Problem with STM32F4
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-31 6:33 AM
Hello guys,
I have problem with bootloader on STM32F427xx.
Bootloader: 0x08000000 ---128Kb
APP: 0x08020000 ----512Kb
In Linker Script for App, the ResetHandler located at
.start 0x08020200 :
{ . = ALIGN(4); KEEP(*(.start)) /* Startup code */ . = ALIGN(4); } > FLASHbut when I tried to executed these:
#define APPLICATION_ADDRESS (0x08020000UL)
pFunction Jump_To_Application;
uint32_t JumpAddress;SCB->VTOR = FLASH_BASE | 0x20000;
/* Initialize user application's Stack Pointer */
__set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS);/* Jump to user application */
JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4 + 0x200); Jump_To_Application = (pFunction) JumpAddress;Jump_To_Application();
I couldn't jump into App section.
Can you help me pls, thanks!
PS: I use Jlink Debugger.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-31 3:57 PM
I tested it with the code above and it works fine.
#define APPLICATION_ADDRESS (uint32_t)
0x08020000
//
Bootloader
Test code{
printf('\n\n JUMP USER FW -->\n'); /* Test if user code is programmed starting from address 'APPLICATION_ADDRESS' */ if (((*(__IO uint32_t*)APPLICATION_ADDRESS) & 0x2FFE0000 ) == 0x20000000) { /* Jump to user application */ JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4); JumpToApplication = (pFunction) JumpAddress; /* Initialize user application's Stack Pointer */ __set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS); JumpToApplication(); } }// Application
Test code
-> system_stm32f4xx.c SystemInit() function (
Application project )
VECT_TAB_OFFSET : The value needs to be modified in application project.
#define VECT_TAB_OFFSET
0x20000
Please test it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-31 4:21 PM
Why on earth do you have the +0x200 in there?
JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4 + 0x200);
You are loading an ADDRESS from the vector table, the ADDRESS should point to the ResetHandler
Also, this would be less ambiguous
SCB->VTOR = APPLICATION_ADDRESS;
If you are unsure about addresses you can print them out, or step the code with a debugger. You can look at the .MAP file of the APP to understand if you are going to the right functions
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-02 7:44 AM
I have a configuration similar to you with a custom flashloader located at 0x0802 0000 and my application at 0x0804 0000. The way I found easier for us is to reconfigure the option bytes and reset the CPU.
here is my function to do it
void StartIPLB2FlashLoaderCode(void)
{
HAL_StatusTypeDef Status = HAL_ERROR;
//Address = (<ADDR_BOOT_PIN_1> << 16) | <ADDR_BOOT_PIN_0>
uint32_t Address = 0x00400088;
//Clear Any Pending Flash Flags
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR |\
FLASH_FLAG_PGAERR | FLASH_FLAG_PGPERR| FLASH_FLAG_ERSERR);
if(HAL_FLASH_Unlock() == HAL_OK)
{
//Set Half-Word write operation
FLASH->CR &= CR_PSIZE_MASK;
FLASH->CR |= FLASH_PSIZE_HALF_WORD;
HAL_FLASH_Lock();
if(HAL_FLASH_OB_Unlock() == HAL_OK)
{
if(FLASH_WaitForLastOperation((uint32_t)FLASH_TIMEOUT_VALUE) == HAL_OK)
{
FLASH->OPTCR1 = Address;
Status = HAL_FLASH_OB_Launch();
}
HAL_FLASH_Lock();
}
}
if(Status == HAL_OK)
{
HAL_NVIC_SystemReset();
}
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?