Bluepill HC4067 via Arduino IDE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-17 3:09 AM
Hi everyone. I´d like to use a HC4067 mulitplexer to expand analog inputs on a bluepill. I´m using Arduino IDE to program the thing. But I can´t get reliable results. The values are jumping up and down or not reacting to input (potentiometer).
I´m wondering if using a HC4067 is restricted to certian pins?? I´m trying to use:
int s0 = PB4;
int s1 = PB3;
int s2 = PA15;
int s3 = PA12 ;
SIG = PA4;
I´m powering the HC4067 with 3.3 V and have grounded all inputs except input 1. I get fluctuating readings and POT on input 1 isn´t doing much, although I should see 0-4096.
Any help appreciated. Keep in mind ... newbie here. Or father with just occasional spare time trying to build an RC transmiiter for his son.
Before you ask: I use these pins because there are already other things going on on the board...NRF24 transmitter, Oled, etc.
This code is just a test setup.
//Mux control pins
int s0 = PB4;
int s1 = PB3;
int s2 = PA15;
int s3 = PA12 ;
//Mux in "SIG" pin
int SIG_pin = PA4;
void setup() {
pinMode(s0, OUTPUT);
pinMode(s1, OUTPUT);
pinMode(s2, OUTPUT);
pinMode(s3, OUTPUT);
digitalWrite(s0, LOW);
digitalWrite(s1, LOW);
digitalWrite(s2, LOW);
digitalWrite(s3, LOW);
Serial.begin(9600);
}
void loop() {
//Loop through and read all 16 values
//Reports back Value at channel 6 is: 346
for (int i = 0; i < 16; i ++) {
Serial.print("Value at channel ");
Serial.print(i);
Serial.print("is : ");
Serial.println(readMux(i));
delay(100);
}
}
int readMux(int channel) {
int controlPin[] = {s0, s1, s2, s3};
int muxChannel[16][4] = {
{0, 0, 0, 0}, //channel 0
{1, 0, 0, 0}, //channel 1
{0, 1, 0, 0}, //channel 2
{1, 1, 0, 0}, //channel 3
{0, 0, 1, 0}, //channel 4
{1, 0, 1, 0}, //channel 5
{0, 1, 1, 0}, //channel 6
{1, 1, 1, 0}, //channel 7
{0, 0, 0, 1}, //channel 8
{1, 0, 0, 1}, //channel 9
{0, 1, 0, 1}, //channel 10
{1, 1, 0, 1}, //channel 11
{0, 0, 1, 1}, //channel 12
{1, 0, 1, 1}, //channel 13
{0, 1, 1, 1}, //channel 14
{1, 1, 1, 1} //channel 15
};
//loop through the 4 sig
for (int i = 0; i < 4; i ++) {
digitalWrite(controlPin[i], muxChannel[channel][i]);
}
//read the value at the SIG pin
int val = analogRead(SIG_pin);
//return the value
return val;
}
- Labels:
-
STM32duino
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-17 3:15 AM
//loop through the 4 sig
for (int i = 0; i < 4; i ++) {
digitalWrite(controlPin[i], muxChannel[channel][i]);
//read the value at the SIG pin
int val = analogRead(SIG_pin);
}
try this
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-17 3:25 AM
tried. Now I get near stable 0 on all inputs. If I let just one input pin on the HC4067 float I get garbage on all inputs. Pulling a pin to 3.3V does noting.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-17 3:44 AM
BTW the orignal code, of course with other pins (S0-3/8-11) and SIG A0, works perfect on a Nano. Values are 0-1023 on input 1. all others stay put at 0.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-17 3:57 AM
well that is something, did you discarded wiring problems? you could share your wiring with us
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-17 4:02 AM
arduino nano is based on ATmega328 thats a 5v microcontroller.
bluepill is based on stm32f103c8 and its a 3v3 microcontroller.
Maybe your Multiplexer is not recognising your digital signals as high, you could try changing the multiplexer vcc down to 3v3.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-17 4:09 AM
for testing purposes I just moved the S0-4 and SIG to a Nano and it worked as expected. I admit It is a breadboard mess, but I´ve been checking the wiring for hours now. Thats why my initial thought was I probably could not use
int s0 = PB4;
int s1 = PB3;
int s2 = PA15;
int s3 = PA12 ;
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-17 4:11 AM
I´ve been running the STM setup and the multiplexer solely on 3V3. Althtough the pins I use o the STM are 5V tolerant.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-17 4:14 AM
5v tolerant means they will accept 5v input without burning, they wont do 5v output.
This looks like a wiring problem or a Voltage gpio problem.
You can try reading adc inputs with the stm32 and doing de digital logic with wires to 3v3, to corroborate this.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-17 6:08 AM
it is really weird. I´ve redone the whole wiring and not matter what I try it isn´t working. Right now I have a POT only on Channel 15 and all others to ground. But the readings of all channels are affected by the POT. Could it be a similar issue to what I had with an i2C display? Had to add 4K7 pullups before it wanted to display anything.