2023-06-20 6:03 AM - edited 2023-06-20 6:05 AM
Hello there! I am using the B-L4S5I-IOT01A board. After setting up the AWS process, I have opened tera term to configure the device. After I configured the tera term once I press the reset button on the board, no information is being displayed on the virtual terminal. Can anyone help me resolve this issue?
2023-06-21 1:25 PM
Hello @DDutt.3 ,
Did you try the available example within X-CUBE-AWS package?
I recommend you the following resources:
Thanks
Imen