cancel
Showing results for 
Search instead for 
Did you mean: 

Array initialization

luke514
Senior

I know that the question will be trivial, however, I do not understand why the instruction uint8_t dataRx[4] = { 1 }; does not initialize all the elements of an array to 0 ... but only the first one:

stm32 array 2.png

I have programmed little in the last while so I will probably misremember myself, however I was almost convinced that such instruction initialized the whole array to zero ... as also written here.

The two arrays in the picture (let's consider only array2) are inside a function of a sensor library that, at this point, I don't know if it is intended to initialize to 1 only the first element or all the elements of array2 ..

In any case I solved it using:

memset 

 

To recap, is the fact that the uint8_t dataRx[4] = { 1 } instruction does NOT initialize all elements to 0 an error on my part or is this likely to happen on other compilers?

2 REPLIES 2
KnarfB
Principal III

Correct. Only the first element will be initialized (edit: to 1). And yes, its the law: Array initialization - cppreference.com

hth

KnarfB

gbm
Principal

All the elements are initialized, the first one to 1, others to zeros. That's the standard behavior and every compiler must do that.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice