2024-04-04 11:34 AM
I am using STM32CubeIDE 1.15.0, writing code in C, including some assembler code, for the STM32G431.
According to ST's programming manual PM0214 in Section 3.5.1, I should be allowed to use
adc r0, r1, lsl #1
However, gcc barfs (I am using standard gnu18) with the following message:
garbage following instruction -- 'adc r0,r1,lsl#1'
What am I missing?
Solved! Go to Solution.
2024-04-04 12:22 PM
These forms ALL work in KEIL
234 00000008 EB40 0041 adc r0,r1,lsl#1
235 0000000C EB40 0041 adc.w r0, r0, r1, lsl #1
236 00000010 EB40 0041 ADC r0,r0,r1,LSL #1
Will poke GNU/GAS later..
2024-04-04 11:58 AM
You are missing register name before lsl.
2024-04-04 12:22 PM
These forms ALL work in KEIL
234 00000008 EB40 0041 adc r0,r1,lsl#1
235 0000000C EB40 0041 adc.w r0, r0, r1, lsl #1
236 00000010 EB40 0041 ADC r0,r0,r1,LSL #1
Will poke GNU/GAS later..
2024-04-04 1:49 PM - edited 2024-04-04 1:52 PM
Thanks, guys, for helping me out. It works now!
2024-04-04 1:59 PM
The version of GAS I'm using found these latter two were acceptable
121 0034 40EB4100 adc.w r0, r0, r1, lsl #1
122 0038 40EB4100 ADC r0,r0,r1,LSL #1
objdump -d yielded this form, which is the form I'd choose for re-assembly
34: eb40 0041 adc.w r0, r0, r1, lsl #1
38: eb40 0041 adc.w r0, r0, r1, lsl #1
2024-04-04 2:05 PM
I'm a little disappointed than GNU/GAS won't handle the short/truncated version.
I tend to use KEIL / ARMASM to rebuild recovered source, and I do find the syntax differences between tools to be frustrating at times. Although I guess I'd prefer it error than fail to generate the right opcodes