2020-03-26 9:46 AM
The board is needed for a small embedded project with low-power energy required.
Thanks by advance
2020-03-26 11:19 AM
>>Are the Nucleo-F303K8 etc.. equipped with an integrated bluetooth device ?
NO
As I understand it the NUCLEO-32 boards share a common form-factor, but there are manuals presumably with specifics.
2020-04-02 3:13 AM
Thanks for your answer ! ;)
2020-04-02 5:57 AM
Not sure the boards are geared to low power, in the sense they typically have a lot of peripheral devices/components attached
https://www.st.com/en/evaluation-tools/p-nucleo-wb55.html
You might look at feather boards
2020-04-02 7:30 AM
Well, for Nucleo Board you can not say "they typically have a lot of peripheral devices/components attached". But for low power setup, think carefully how the connected ST-Link interacts!