cancel
Showing results for 
Search instead for 
Did you mean: 

ADC1 in STM32H753 gets 0xFFFF as the digital value for HAL_ADC_Start & HAL_ADC_Start_IT & HAL_ADC_Start_DMA.

Ofer
Associate III

I use ADC2 and ADC3 (with HAL_ADC_Start_DMA) with no problem, just having problem with ADC1. I'm using FREE-RTOS. STM32CUBEIDE.

1 ACCEPTED SOLUTION

Accepted Solutions
Ofer
Associate III

Hi

The problem has been solved. The Vref was 1.5V (instead of 3.0V) so the signal was saturated.

Thanks anyway.

View solution in original post

3 REPLIES 3
FBL
ST Employee

Hello @Ofer​,

Could you please share your configuration? Pin configuration, DMA channel ...? IOC file if possible? 

Does conversions are performed sequentially or simultaneously?

Same issue observed without FreeRTOS?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


Ofer
Associate III

Hi dear Mr. Belaid

Attached the ioc file.

I use a simple polling conversion:

for( uint16_t sample_index = 0 ; sample_index < sample_number ; sample_index++ )

{

  HAL_ADC_Start(&hadc1);

HAL_ADC_PollForConversion(&hadc1, 1000);

modulation_feedback_samples[sample_index] = HAL_ADC_GetValue(&hadc1);

  HAL_ADC_Stop(&hadc1);

}

Have the same issue without FreeRTOS.

Thanks

Ofer
Associate III

Hi

The problem has been solved. The Vref was 1.5V (instead of 3.0V) so the signal was saturated.

Thanks anyway.