cancel
Showing results for 
Search instead for 
Did you mean: 

ADC1/ADC2 configuration options differs from ADC3 on STM32H723

elso
Associate III

Hi All,

I want to use two ADCs on STM32H7 configured equal, but using one DMA each, and measuring on different channels. However it seems like the ADC3 have options ADC1 and 2 doesn't have. In this case DMA continuous request.

elso_0-1702646531200.pngelso_1-1702646561545.png

Is this intentional? A workaround?

Best regards!

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Sarra.S
ST Employee

Hello @elso,

>>However it seems like the ADC3 have options ADC1 and 2 doesn't have 

Indeed, please refer to RM0468 where there are two paragraphs one for ADC1/ADC2 and the other for ADC3

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Sarra.S
ST Employee

Hello @elso,

>>However it seems like the ADC3 have options ADC1 and 2 doesn't have 

Indeed, please refer to RM0468 where there are two paragraphs one for ADC1/ADC2 and the other for ADC3

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.