2015-10-28 09:30 AM
My fault. Post invalid. I looked at the schematics of the nucleo boards and mistook SD_VREF+ for VREF+. Sorry.
Hi.
In STM32F334R8 PB12 is connected to VREF+ for the ADCs.I have made a HW design using PB12 for other purpose. However I need to use ADC2 but I did not find any way to switch the ADC reference internally (!) to VDDA. It looks as if I must cut a wire on my board and change my HW design only to connect PB12 to VDDA. It that so?Coming from other �C vendors I am used to ADCs that may run on VDDA as a reference or on a dedicated internal Reference. Any hints? #stm32-stm32f334-adc-reference