2025-03-20 5:07 AM
I am just wondering how it is possible that 3 adc gave me the very same value, if I change the channel and their rank are different.
Thanks for all.
2025-03-20 5:21 AM
@carlesls2 wrote:I am just wondering how it is possible that 3 adc gave me the very same value
Are they all connected to the same thing?
Please see: How to write your question to maximize your chances to find a solution
and: How to insert source code - not as images
2025-03-20 5:59 AM
When converting a single channel in fully configurable mode, rank 1 is the only channel converted.
Two of your three pictures are the same. The other one configures rank 3 which isn't converted.
2025-03-20 6:06 AM
Almost the same value...
2025-03-20 6:20 AM - last edited on 2025-03-20 6:25 AM by Andrew Neil
Merged from separate thread
I was just wondering... If an adc is burned inside a stm32g051g8, should all the values that the ADC from different channel be the same or quite similar?
Thanks for all.