2022-06-07 6:18 PM
I want to perform a timer interrupt using the output comparison mode.
When the frequency is set to 2000Hz, ARR : 20, CCR1 : 25, I think that interrupt does not occur because ARR <CCR1, but interrupt occurs. Why do interrupts occur?
Solved! Go to Solution.
2022-06-07 11:09 PM
2022-06-07 11:09 PM
2022-06-07 11:50 PM
I confirmed that it is described in the reference manual.
I overlooked it because it was not mentioned in the Japanese version of the manual.
Thank you for your cooperation.
2022-06-08 1:37 AM
> I overlooked it because it was not mentioned in the Japanese version of the manual.
Maybe this should be fixed, then. I am not sure where should this be reported, maybe through your FAE?
@Imen DAHMEN , what is the proper way here?
Thanks,
JW