2017-04-17 03:51 AM
Hi,
Are there 64-bit libraries available (now or in future) for ST-LINK/V2?
Thanks
2017-04-17 09:29 AM
Hi
ali.mehar
,Download this version
v 1.02:ST-LINK, ST-LINK/V2, ST-LINK/V2-1 USB driver signed for Windows7, Windows8, Windows10(for 32 bits and 64 bits).Imen
2017-04-17 12:09 PM
Hi Imen,
Thank you for responding.Excuse my ignorance on the matter but previously I had been using STLinkUSBDriver.dll from STM32 ST-Link utility (installation obtained from STSW-LINK004) to detect the ST-Link/v2 debug interface other than installing the drivers. Wouldn't it be required to have 64-bit version of this dll as well?
Thanks
M. Ali
2017-04-17 02:18 PM
No, and most things using the DLL are likely 32-bit also