GPIO to SRAM using DMA. Is it possible in STM32?
Hi all,
I am a bit of a newbie to the microcontrollers world and trying to work in my first real project, in which I want to capture data from an external ADC and store it into the embedded SRAM for post processing.In my initial test I am using an STM32F207 with the Nucleo evaluation board. I configured a GPIO port F as input, just put some random 1s and 0s on the port and transfer it to memory simply by creating an array and copying the GPIO IDR value into the respective elements of the array, a very simple loop as follows:
unsigned int data_gpiof[1024] = {0};
unsigned int i = 0; while (i < 1024) {data_gpiof[i] = *((unsigned int*)0x40021410U);
++i; }In the code, 0x40021410U is the address of the GPIO port F IDR. It works just fine, but the loop takes 13 clock cycles, which is probably too slow for my application.
I was therefore looking for ways to optimize this, and was thinking whether it is possible to use DMA. From the datasheets, STM32 controllers do not support DMA between GPIO and memory, so I was wondering if that is really the case?
It is possible maybe to configure DMA for memory to memory transfer and just set the IDR of the relevant GPIO port?
Otherwise, is there any improvement that you can think of for the code above to make it more efficient?
I can see that the instruction data_gpiof[i] = *((unsigned int*)0x40021410U); involves many steps at assembly level. I assume there is probably a more efficient way to achieve the same result.
Any advice is welcome.
Thanks in advance!
#DMA, GPIO