2017-01-23 02:01 PM
The 32F413HDISCOVERY webpage, and also the data brief DocID029964 Rev 1, both say the kit has:
USB OTG HS with Micro-AB connector
however, the STM32F413 has 'only' an USB OTG FS.
Also, on the picture of the DISCO's PCB in the databrief it can be seen an overlay text 'USB_OTG_FS' next to said microAB connector.
Please comment.
Thanks,
JW
Solved! Go to Solution.
2017-01-24 12:58 AM
Hi Jan,
Thanks for highlighting this discrepancy: you are right; only USB_OTG_FS is available in STM32F413ZH.
This is noted and will be fixed soon (in both web page and databrief).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-01-24 12:58 AM
Hi Jan,
Thanks for highlighting this discrepancy: you are right; only USB_OTG_FS is available in STM32F413ZH.
This is noted and will be fixed soon (in both web page and databrief).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.