2020-11-25 8:48 PM
Hello,
quite new to STM32 platform (used during the university time, then moved to a competitor for work). I am now trying to come back. In particular I want to set up a small IoT project.
I bought a 32F413HDISCOVERY board and I am using STM32CubeIDE. I would like to use AWS IoT so I have downloaded X-CUBE-AWS 1.4.1 and I went through the documentation UM2178 rev 1 (the latest rev 4 is only for X-CUBE-AWS 2.0 and I cannot find the other revisions).
I have all set up from AWS point of view. And now I am stuck.
I have tried importing the project contained in the zip file for my board and compile, but I get errors. In the manual is written that something show be flashed, but it is unclear which file.
Can I get some indications on how to go on? Is it a problem of the IDE (that did not exist when the manual was written)?
Thanks in advance
Davide
Solved! Go to Solution.
2020-11-26 7:37 PM
Thanks for the correction, but it was not the solution. I am not an expert in bash scripts, but based on the error I posted before, the script goes to the "else" section, so the problem is not with the PATH definition only. I have removed the check if the script is running on Windows. Now the script looks like below and it is working! Thank you a lot.
if [ $ret == 0 ] && [ $# == 5 ]; then
echo "Generating the global elf file SBSFU and userApp"
echo "Generating the global elf file SBSFU and userApp" >> $projectdir"/output.txt"
# Set to the default installation path of the Cube Programmer tool
# If you installed it in another location, please update PATH.
PATH="~/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin":$PATH > /dev/null 2>&1
programmertool="STM32_Programmer.sh"
command=$programmertool" -ms "$elf" "$headerbin" "$sbsfuelf
$command >> $projectdir"/output.txt"
ret=$?
fi
2020-11-26 1:08 AM
Hello
what errors do you have during compilation ? Are you on a Windows PC or Linux or Mac ?
the file to flash with STM32CubeProgrammer should be under Projects\STM32F413H-Discovery\Applications\Cloud\AWS\SW4STM32\PostBuild\SBSFU_STM32F413H-Discovery_AWS.bin
Alternatively if STM32CubeIDE project compiles without error it is possible to debug the project with STM32CubeIDE using "Debug As ... STM32 Cortex M C / C++ application". In that case it's STM32CubeIDE that flashes the .elf file under Debug/.
there's also a precompiled binary delivered under Projects\STM32F413H-Discovery\Applications\Cloud\AWS\Binary\ but it was compiled with IAR EWARM ( not STM32CubeIDE).
there's an updated manual for X-CUBE-AWS 1.4.1 at https://github.com/STMicroelectronics/x-cube-aws (in Doc directory)
2020-11-26 1:43 AM
Thank you Guillaume.
I have spent some other time. Flashing (via dang and drop) the bin already in the zip file works and I see the bootload starting.
I am using Linux. The importation of the System Workbench project to STM32CubeIDE gives no error. When I compile all, at the end I receive the following error. Ideas? Should be not folder permissions
arm-none-eabi-size STM32F413H-Discovery_AWS.elf
text data bss dec hex filename
194064 736 124792 319592 4e068 STM32F413H-Discovery_AWS.elf
Finished building: default.size.stdout
arm-none-eabi-objdump -h -S STM32F413H-Discovery_AWS.elf > "STM32F413H-Discovery_AWS.list"
Finished building: STM32F413H-Discovery_AWS.list
arm-none-eabi-objcopy -O binary STM32F413H-Discovery_AWS.elf "STM32F413H-Discovery_AWS.bin"
Finished building: STM32F413H-Discovery_AWS.bin
arm-none-eabi-objcopy -O binary "STM32F413H-Discovery_AWS.elf" "STM32F413H-Discovery_AWS.bin"
arm-none-eabi-size "STM32F413H-Discovery_AWS.elf"
text data bss dec hex filename
194064 736 124792 319592 4e068 STM32F413H-Discovery_AWS.elf
"../../../../../BootLoader_OSC/2_Images_SECoreBin/SW4STM32/postbuild.sh" "../.." "./STM32F413H-Discovery_AWS.elf" "./STM32F413H-Discovery_AWS.bin" "1" "bigelf"
/bin/sh: ../../../../../BootLoader_OSC/2_Images_SECoreBin/SW4STM32/postbuild.sh: Permission denied
make[1]: *** [makefile:102: post-build] Error 126
make: *** [makefile:64: all] Error 2
"make all" terminated with exit code 2. Build might be incomplete.I'll give a look at the updated manual, maybe I find something.
Thanks again
Davide
2020-11-26 2:05 AM
Apparently the SBSFU postbuild script doesn't have executable bit set on Linux.
This post-build operation is very important to obtain a full binary with secure bootloader and the application merged together.
try to do a "chmod +x" on Projects/STM32F413H-Discovery/Applications/BootLoader_OSC/2_Images_SECoreBin/SW4STM32/postbuild.sh
2020-11-26 2:38 AM
That helped. I run again and I had to install ecdsa and pycryptodomex to fix two other issues. However, now I have a new error. Should I conclude that the postuild works only under Windows?
arm-none-eabi-size "STM32F413H-Discovery_AWS.elf"
text data bss dec hex filename
194064 736 124792 319592 4e068 STM32F413H-Discovery_AWS.elf
"../../../../../BootLoader_OSC/2_Images_SECoreBin/SW4STM32/postbuild.sh" "../.." "./STM32F413H-Discovery_AWS.elf" "./STM32F413H-Discovery_AWS.bin" "1" "bigelf"
prepareimage with python script
Generating the global elf file SBSFU and userApp
fix access path to STM32_Programmer_CLI.exe
../../../../../BootLoader_OSC/2_Images_SECoreBin/SW4STM32/postbuild.sh: line 93: -ms: command not found
-ms ./STM32F413H-Discovery_AWS.elf ../../PostBuild/STM32F413H-Discovery_AWSsfuh.bin /home/davide/STM32CubeIDE/proto_1/STM32CubeExpansion_Cloud_AWS_V1.4.1/Projects/STM32F413H-Discovery/Applications/BootLoader_OSC/2_Images_SBSFU/SW4STM32/STM32F413H_DISCOVERY_2_Images_SBSFU/Debug/SBSFU.elf : failed
make[1]: *** [makefile:102: post-build] Error 1
make: *** [makefile:64: all] Error 2
"make all" terminated with exit code 2. Build might be incomplete.
2020-11-26 3:19 AM
It seems that is a common issue but still I cannot solve it https://community.st.com/s/question/0D53W0000091jd7SAA/problem-with-sbsfustm32l496gdiscoverycloudawsv140bin-pl496gcell02
I have installed STM32CubeProg in /home/davide/STM32Microelectronics and tried to fix the part in the postbuild.sh file (line 85 on) as following, but still doesn't work. Path typing error or still something missing?
# Set to the default installation path of the Cube Programmer tool
# If you installed it in another location, please update PATH.
PATH="/home/davide/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/";$PATH > /dev/null 2>&1
programmertool="STM32_Programmer_CLI.bin"
2020-11-26 5:44 AM
On Linux, use a colon (":") to separate the directories in the PATH:
PATH="/home/davide/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin":$PATH > /dev/null 2>&1
2020-11-26 7:37 PM
Thanks for the correction, but it was not the solution. I am not an expert in bash scripts, but based on the error I posted before, the script goes to the "else" section, so the problem is not with the PATH definition only. I have removed the check if the script is running on Windows. Now the script looks like below and it is working! Thank you a lot.
if [ $ret == 0 ] && [ $# == 5 ]; then
echo "Generating the global elf file SBSFU and userApp"
echo "Generating the global elf file SBSFU and userApp" >> $projectdir"/output.txt"
# Set to the default installation path of the Cube Programmer tool
# If you installed it in another location, please update PATH.
PATH="~/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin":$PATH > /dev/null 2>&1
programmertool="STM32_Programmer.sh"
command=$programmertool" -ms "$elf" "$headerbin" "$sbsfuelf
$command >> $projectdir"/output.txt"
ret=$?
fi