cancel
Showing results for 
Search instead for 
Did you mean: 

"self downloading" firmware via USB

PNova.2
Associate II

Hello
is it possible for the microcontroller with USB OTG to download the program memory from the USB stick itself?
In other words, change the firmware simply by connecting a USB stick with a .bin file and perhaps by resetting the component.

So far I have solved it using two MCUs. One only reads the .bin file from the USB and then uploads it to the target device via the usart bootloader, but this seems too impractical to me.

1 ACCEPTED SOLUTION

Accepted Solutions
MM..1
Chief II

If you ask for system boot solution then no, But you can use own bootloader for this...

View solution in original post

2 REPLIES 2
Andrew Neil
Evangelist III

Sure - it's just a way to get the data into the microcontroller.

MM..1
Chief II

If you ask for system boot solution then no, But you can use own bootloader for this...