2016-03-01 11:02 PM
Hei there
Is there any working mp3 player using this eval board ?Right now I try helix mp3 decoder but cannot compile using keil v4.There are some error on assembly.h i cannot understand.Please guide me thanks. #mp3-stm32f4 #mp3-player2016-03-07 03:53 AM
wrong memory map in linker script.
2016-03-07 08:30 PM
Hellow dembek
thank for your reply. I never change linker script it still same by default except --fpu part but it didn't affect anything.-cpu Cortex-M4.fp *.o
--entry Reset_Handler --first __Vectors --strict
--fpu=vfpv4_d16 --summary_stderr --info summarysizes --map --xref --callgraph --symbols
--info sizes --info totals --info unused --info veneers
--list ''.\MP3Player.map''
-o MP3Player.axf
I am also looking mapping file and it seem normal. Maybe there are something that i don't know about.
2016-03-08 08:10 AM
Maybe there are something that i don't know about.
The linker script (GUI or Scatter File) needs to describe the FLASH as being at 0x08000000, not ZERO or 0x8000The flashing software says it can't write at 0x8000, because there is no flash memory there. Reflect on what the errors tell you.2016-03-09 05:48 PM
Yup its working now. But still cannot play the mp3 lol.
Thank you all for guiding me step by step 🙂2016-03-10 12:10 AM
Now I face debug problem on keil. It said cannot access memory.
I trace and it stuck in startupxxxx.asmReset_Handler PROC
EXPORT Reset_Handler [WEAK]
IMPORT __main
IMPORT SystemInit
LDR R0, =SystemInit
BLX R0
LDR R0, =__main
BX R0 ;
got stuck here it goes to hard fault
handler
ENDP
I try to lower debug frequency but still nothing.
2016-09-04 06:12 AM
Hello,
my compilation is successful. But you can not hear the music. Check where the errors are. ________________ Attachments : mp3sample20120318-chiny.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I06a&d=%2Fa%2F0X0000000bTU%2F3EPNVxx6qKtVulMJykcMwsnFhEbaXhAF3PC7P5jZqQs&asPdf=false2016-09-04 06:30 AM
Not sure there are a wealth of people here to review the code. Would suggest two courses of action, a) write the decoded PCM data into a file, or .WAV file, and confirm the audio signal is present, and b) prove that a sine-wave data sample generates the frequency output expected on the audio channel(s). Instrument the decode process to confirm it is working, like the PCM data is 10x bigger than the input MP3 @ 128kbps for example.