2020-04-17 5:07 PM
I bought the NUCLEO-F303RE MCU and the STEVAL-IPM15B 3Sh evaluation board and I want to use it with motor Profiler 5.4.3 software. My only issues is that I don't know where to find the pins that I have to associate between these two boards. If someone can help me with that, it would be really appreciated !
thanks a lot
Jeremy
2020-09-11 2:54 AM
Dear JLort.1
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-10-14 2:01 PM
Dear @JLort.1
I guess you don't have to solve this problem anymore, therefore I consider this post closed.
If not, feel free to reopen it by posting a new answer.
Best regards
Laurent Ca...
2021-06-27 6:35 AM
I have the same problem. But ı can't solved it.