cancel
Showing results for 
Search instead for 
Did you mean: 

Where can I find HW deadtime setting?

DMeie.2
Senior II

We're using a driver that inserts a deadtime by hardware.

It is not clear to me how I have to configure that into the MCWB firmware to get ADC measurement working properly.
I see three deadtime-related settings:
- "minDeadTime" property in the "PhaseVoltageGeneration" feature of the Motor Control Boards Description
- "deadTime" property of the "DrivingHighAndLowSides" HW variant (this reads like this is a fixed deadtime inserted by the PWM timers)
- "SW dead-time" setting in the FOC wizard

I couldn't find a proper documentation for any of those.

What do these values do?
Which of those settings is the correct one for my case?

0 REPLIES 0