Skip to main content
Associate
November 19, 2024
Solved

Troubleshooting of STEVAL-IHM028V2

  • November 19, 2024
  • 5 replies
  • 1961 views

Hello,

While I did tests with my motor control STEVAL-IHM028V2, I made a mistake to schort-circuit the three-phase output ! Then, I smelled a burning smell and no voltage is given in the three-phase output . When I checked the bottom face of the device, I noticed that some resistors (R74, R75 and R69) are burned (see attached images). Also, the W7 and W8 jumpers are short-cicuited. How could I fix this issue ?

N.B. The schematic of the STEVAL-IHM028V2 is attached.

Cordially

Tarek

 

This topic has been closed for replies.
Best answer by GMA

Hello @Tarek_ben,

You can try to replace all of these components (resistors/jumper).
Set a conservative limitation current on your external DC supply.
Verify that DC voltages are correctly generated on the board. 
Monitor the current consumption when relaunching test.

5 replies

Tarek_benAuthor
Associate
November 21, 2024

Any answer about this ?

GMA
ST Technical Moderator
November 26, 2024

Hello @Tarek_ben,

On your IHM028V2.jpg picture, nothing seems to be burned... 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Tarek_benAuthor
Associate
November 26, 2024

Thank you for the answer.

If you zoom in on the resistances R74, R75 and R69, you can see a black line in the middle of these resistances.