cancel
Showing results for 
Search instead for 
Did you mean: 

When will ST Motor Profiler support EVSPIN32G4?

WSega.1
Associate II

The EVSPIN32G4 is not an option when you 'select hardware' in the latest version of the Motor Profiler (5.Y.4). Will it be supported in an upcoming release? Also, is there any plan to support higher RPM profiling? The limit is 16kRPM right now.

1 REPLY 1
GMA
ST Employee

Dear WSega,

Firstly, we would like to sincerely apologize for the delay in replying to your post.
If your point is still pertinent, on future 6.2 release, you will be able to use it for profiling feature.
On current versions, the displayed 16K RPM max speed it is only an example, you can set an higher value.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA