2025-04-02 3:58 AM - last edited on 2025-04-02 7:04 AM by Andrew Neil
Hi All,
I am beginner to drones. We assembled one drone using STEVAL FCU. 002. board , recommended set. of motors and. propellers along with battery.
We Chose different. frame. than. one recommended . It is smaller in size.
While flying , vertical take. off. could. not be achieved.
Can someone guide please ?
Motor connections , Clock wise. , anti clock wise in reference. to alignment. of. the boards are checked. already.
It is ST board. so. come equipped with all driver , frimware etc.
Thanks in advance.
Early and accurate response is. appreciated.
Regards,
2025-04-02 10:33 PM
Albeit, if your comment was for ready made frame, we already got one 3D printed using STL file from ST. If it still gives trouble , than we will go with ready made supplied by ST.
2025-04-07 9:13 AM
One more observation..
In help section, There is mention of VERTICAL TAKE OFF and VERTICAL LANDING button in ST_BLE_DRONE application.
But in App GUI , we could not find any of them.
Now, we have got the frame as recommended by ST.
And we will assemble using that.
I doubt that without VERTICAL TAKE OFF button , how it will gain an altitude lift.
Regards,
2025-04-16 6:23 AM
Dear All,
I want to reopen this case. Post last interactions, we got frame as per design of ST ( STL file for 3D printing ) and used the same to reassemble the drone.
Unfortunately , result is not achieved.
Drone does not take off even up to 1 feet and flies in unpredictable directions.
No clear control on flight of drone.
We fail to identify even right area of problem.
Request you people to suggest steps for troubleshooting.
Regards,
Madhu Dave
2025-04-16 6:48 AM
@mmdave1 wrote:Dear All,
I want to reopen this case.
You can unmark the solution:
@mmdave1 wrote:we got frame as per design of ST ( STL file for 3D printing ) and used the same to reassemble the drone.
So you didn't use an actual frame supplied by ST ?
And you haven't answered @Peter BENSCH's question: "which propeller with which tilt did you use where?"
2025-04-16 11:23 PM
Hi Andrew,
I have updated in between .And propellers and motors are again the ones recommended by ST.
Please see below link for details on that.
Now, we are ordering the frame from ST ( original one by ST ).
Besides that , can you please help getting answers to below doubts :
1. Whether ST_BLE_DRONE app is the right tool to control the drone or shall we order REMOCON handheld remote unit to control the drone ?
2. In ST_BLE_DRONE app , we could not find Vertical take Off button where as in the HELP section of the application , we can observe the reference in this regard .
3. Is there any proper user operation guide for ST_BLE_DRONE application ? We may be making mistake even on how to fly the drone .
Regards,
Madhu Dave
2025-04-17 1:19 AM
@mmdave1 wrote:propellers and motors are again the ones recommended by ST.
That still doesn't answer @Peter BENSCH's question!
2025-04-21 6:23 AM
Ok... We have ordered original frame getting supplied by ST. And we will check.
Regarding propeller , we could get only length of it . Tilt angel is not provided even in supplier's data sheet.
Hope , I am not missing any question which I shall answer.
Regards,
2025-04-22 8:05 AM
hello i have exactly the same problem.
2025-04-23 11:00 PM
Hi Rania1,
Please let us know if you achieve any progress.
Similarly , we will also let you know.
Regards,
2025-04-24 4:03 AM
We also have the same problem.
We are making a FCU based on STEVAL-FCU001V2 as a study project. We originally ordered the STVEAL-FCU001V2 via digikey from this link: "https://www.digikey.in/en/products/detail/stmicroelectronics/STEVAL-FCU001V2/22522577", 3D printed the STDRONE002 frame and ordered the 8520 motors and 65mm propellers from this link: "https://robu.in/product/65mm-blade-propeller-prop-8520-cw-ccw-coreless-brushed-motor-indoor-racing-drone-quad-copter/". We are using the exact battery that ST recommended "3.7v 600mAh and 25C discharge rating" purchased from this link: "https://robu.in/product/bonka-3-7v-600mah-25c-1s-lithium-polymer-battery-pack/". But to no extent did it even took off. And in the rare cases that our drone took off, it spined rapidly in the yaw axis.
Any help would be appreciated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.